Hi,
I'have a test circuit for LM2903B.
VCC :3.3V (0.1uF decoupled)
IN- : Voltage reducing from 1.65V to 1.4V (in 15seconds)
IN+: 1.5VDC (Voltage divider from 3.3V)
OUT:2.2kohm pull-up from 3.3V
OUT: Load resistor 39k from Out pin to GND
OUT: No installed output capacitor
Hysteresis resistor: Not Installed
My output voltage starts from 0.051V to 0.4V and sudden change from 0.4V to 1.9V and 3.2V (with decresing +IN. pin)
1) How does the output voltage increase from 0.051 to 0.4V although IN- is bigger than IN+?
2) Why does output voltage increase slowly although IN+ is bigger than IN-?
3) Why is there a transition band from 0V to VCC?
Please, provide explanation in details.