Dear Sir or Madam,
I have a question about the TLV2333IDR operational amplifier:
What is the permissible differential input voltage without destroying the OPV?
Is it enough to limit the input current to max. 10 mA as described in chapter 8.3.2 Fig. 18?
In Fig. 20 it is visible that the OPV contains two clamp diodes and two 10 kOhm resistors to protect against too high differential input voltages.
In other data sheets, e.g. the OP07CD, there is a precise specification for the differential input voltage, e.g. Differential input voltage = max. ±30 V.
Thank you very much for your help.
With kind regards
Manuel Christ