Other Parts Discussed in Thread: OPA3690
Team,
Can you please to identify if we have some possible better alternatives to OPA690 for the below use case?
Voltage feedback OP-Amp for:
Freq. range 0Hz…30MHz
Input: Differential input with V_CM~3.5V and -V_signal_pp=1,8V
Output:
single ended and capable to drive a 50R load.
Output voltage max. 2Vpp (or more)
Had first look at OPA690 (or OPA3690, just to build an instrumental amplifier with 3 OP-Amps, toconvert a diff. input signal into a single ended output).
Key parameters of the OPA690 are:
-It can be supplied by +/-6V (that is nearly 4Vpp @ 50R at the output are possible)
-Bandwidth is beyond 160MHz (that is enough for the 30MHz application)
-Current output is above 140mA (enough to drive a 50R load
-It does have an input noise density of about 5.6nV/√Hz (could be better)
Is there an even better alternative than OPA690 that match those key parameters and meet the above input/output/freq requirements?
Thanks in advance,
A.