Hi,
This is Allen Hu from Shenzhen China,I have a question about TLV3603,Please see the following shcematic for details.
Where is :
-The range of AC_IN is DC 5.6V ~ 19V;
-AC_DC_5V2 is 5.2V;
The circuit will monitor the input voltage of IN+ is greater than 0.4V or not. if YES,OUT will output "high"then pull-down"LE"and keep "high".
Could you please kindly help to review if the circuit is doable or not.if can not,How to improve it or which part is preferred.
Looking forward to your feedback/comfirmation.
Thanks so much
Allen Hu