Hello
I am designing comparator circuit used LM311.
I would like to confirm whether there is a problem under the following conditions.
(1) Power supply voltage to Vcc+ pin is +15V
(2) Power supply voltage to Vcc- pin is -15V
(3) Input voltage to IN+ pin is +24V or 0V
(4) Input voltage to IN+ pin is +7.5V(Fixed voltage)
* I am concerned about the voltage on the IN+ pin exceeding the Vcc+ pin voltage.
Regards,
MESH