This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA240-Q1: INA240-Q1

Part Number: INA240-Q1
Other Parts Discussed in Thread: INA240

Hi Team,

I am using INA240A1-Q IC in my project.

Circuit:

  • Shall i use Rs ( R0505 & R0506) value from 330 ohm (>300ohm) in place of 30 ohms ??
  • Are these values impacting the any gain error and CMRR value?? Are there any other parameter effects?

  1. For 30.01 ohm ==> Common mode cut-off frequency = 241MHz and Differential mode cut-off frequency = 12.06MHz.
  2. For 330 ohm    ==> Common mode cut-off frequency = 21.9 MHz and Differential mode cut-off frequency = 1.10MHz.