This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRF0206-SP: Can be used w/ DC coupling?

Part Number: TRF0206-SP

Hello,

The datasheet says 10 MHz to 6.5 GHz 3-dB BW, but page 8 s-parameters plots are from DC.
Can TRF0206-SP be functional with DC coupling configuration, though many parameters are not specified below 10MHz.
Any concerns with DC coupling? What do customers have to take care about at DC coupling?

Best regards,

K.Hirano

  • Hi Kazuhiko,

    The TRF0206-SP is unable to pass through true DC signals. The graph is a visual misinterpretation as the Fmin (10MHz) stops graphically right next to the edge of the graph. We will update our datasheet to prevent this visual misinterpretation.

    Thanks,
    Jon