This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV170: Can I input voltage Vi over VCM(common-mode voltage)in Inverting Amplifier Circuit

Part Number: TLV170
Other Parts Discussed in Thread: OPA627, OPA171

Hello everyone,

      I was wondering recently, when I adjusted the resistance to set the gain in the figure below to G=-0.5, could I set the input voltage to Vi = -18V.In theory, it is beyond the scope of VCM, but in practice and simulation, there is no problem.

      Thanks for answering my questions!

    

  • Hello Yuqi,

    VCM is the voltage on the op amp input pins. It does not refer to the input voltage on the far side of the resistor. 

  • Hello Ron

        Thank you for your answer,I want to know the theory. Before the operational amplifier is stabilized, I feel that this Vi will enter into the op amp through the input pin, so I have questions about Vi and VCM in Low gain Inverting Amplifier Circuit When Vi is greater than VCM.

        Kind Regards!

  • Hi Yugi,

    it's always critical when the input voltage exceeds the supply voltages of an OPAmp. Not only phase inversion can happen, but also latch-up, lock-up and even damage.

    In any case, I would add a diode clamp across the inputs of OPAmp as shown in figure 33b of datasheet of OPA627.

    Kai

  • Yuqi,

    In cases where input exist before power up or input changes so fast that op amp can't send enough correction to keep input valid, there can be issues as Kai stated. Depending on the op amp, I might have given this information initially.

    However, OPA171 data sheet mentions that there is no phase reversal and ABS MAX table shows an input current.

    Adding a diode may not bypass all of the input current; the diode is capacitive. If diode is Schottky, it will leak badly at high temperature.