Other Parts Discussed in Thread: AMC1351
Hello,
I'm using this isolated amplifier AMC1351-Q1 to monitor a voltage busbar (1200Vdc max).
I have included a voltage follower between the divisor resistors and the input pin of this isolator amplifier.
See attached capture to check details of the connection.
The intention to do this was to add independency on the impedance between the divisor resistors and the isolated amplifier.
After checking the isolator amplifier datasheet, I wanted to know whether this is redundant and I can get rid off this stage or it can be used without affecting the input impedance of the isolator amplfier (Zinput of isolator amplifier in parallel with Zout of Voltage Follower).
As to input capacitor, in case of use it, does it make sense to move it to the resistor RSNS as it is indicated in the attached capture?

Regards,