Hi team,
Customer sometimes see the VIN- is -1.5V with Vee=GND when using LM2904LVIDDFR.
Is there any opamp which are able to stand this negative voltage without supplying negative voltage?
Regards,
Hayashi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Customer sometimes see the VIN- is -1.5V with Vee=GND when using LM2904LVIDDFR.
Is there any opamp which are able to stand this negative voltage without supplying negative voltage?
Regards,
Hayashi
As far as I know, all opamps have negative clamping diodes, which must be protected.
A series resistor of more than 100 Ω in front of the input would limit the current through the diode to a safe < 10 mA.
Hi Hayashi,
figure 2-7 of this appnote shows a suited protection circuit:
Application Design Guidelines for LM339, LM393, TL331 Family Comparators (Rev. B)
Kai
Hello Hayashi-san,
On front page of the data sheet is "The op amps are stable at unity gain, and do not have reverse phase in overdrive conditions."
Be sure that there is enough input resistance to keep input current well below 10mA , 10mA is in absolute maximum table.