Part Number: OPA602
Other Parts Discussed in Thread: LM6142, TL071
Hi Team,
Good day. I am posting this inquiry on behalf of the customer.
"I am looking for a replacement for OPA602AP.
I would also only like through-hole parts, no soldering is required
I am trying to take an output voltage from an optical sensor and convert that signal to an output signal between 0-1VDC


The min and max voltage of the Optical sensor is between 0.3VDC and 2.8VDC
the main inquiry is a replacement device for OPA602AP
the other information is to give context to the project I am working on and the goal I am trying to achieve
I simulated the circuit using a product that is obsolete and therefore needs something that will do the same thing."
Please help to advise. Thank you for extending your support.
Kind regards,
Marvin