This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH32401: LM32401

Part Number: LMH32401


Hello,

I am using the LM32401 see schematic attached:

LMH34204 + LMH6552 driving the RFSOC.pdf

1. Power to ADC is coming first -so there is 0.7V the common mode voltage)

2. Power of +5V, -5V and 3.3V come later.

The problem that I encounter is that VOC that should be 1.1V is becomes around zero and the output is oscillating. (The deferential voltage on R1 is 1.2V.)

Any comment ?

Sincerely,

Giora