Part Number: OPA2378
Other Parts Discussed in Thread: OPA2387, OPA2335, OPA2391, OPA2369, OPA2348, OPA2186
What can I replace my opa2378 with
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Unfortunately, the only other dual op amp in SOT-23-8 is a micro-power OPA2369 with much lower bandwidth and much higher offset and drift - see below.

That is my dilemma. Will the OPA2378 SOT 23-8 be available soon? There are 19 of these on my current PCBA and at this time it is unfeasible to rev the design.
You might look at the OPA2348, I think that is a close dual in a SOT23-8. RRIO but the Vos is much higher.
Our Precision Amps product line has only two duals in SOT-23-8 package mentioned above but Micheal is correct that the General-purpose Amps product line does have OPA2348 in said package. However, the main issue may be that its specified maximum offset is +/-5mV. OPA2378 is a twenty year-old product with no plans for SOT-23-8 BUT there is a new dual op amp chopper in development that will be available in said package (I don't have RTM date).
Below are other General-purpose SOT-23-8 alternatives:

However, if you use 4.5V or higher supply voltage, we have a direct replacement available right now - OPA2186. Btw, DCN and DDFare both SOT-23-8 packages with the distinction being that DDF has a lower (THINer) profile than DCN.