I am looking into a design that requires several outputs from bipolar instrumentation amplifiers (PGA204) to be connected to a 0 - 5V ADC (ADS8345) - this ADC only accepts inputs in the range of 0 - 5V. I am proposing to use a OPA4376 quad 5V single supply ampifier to buffer the IN-amp outputs to the ADC thus removing the problem of interfacing the bipolar signals (+/-10V) to the ADS8345 input channels. Note an input resistor will protect the amplifier inputs and offset resistor to +2.5REF added to provide a 0 - 5V amplifier output for a +/-10V IN-amp output to the amplifier.
One problem we have however is that any of the IN-amp outputs could saturate when the external sensor input is disconnected and hence an overload voltage (+/-13.5V) could be applied to the OPA4376 amplifiers within the same package. Does anyone know whether the individual amps within the OPA4376 package are isolated from each other such that an overload on any amplifier input will not affect the operation of any non-overloaded amplifiers within the same package, i.e. no channel interaction occurs under all operating conditions.
Secondly, the OPA4376 data sheet gives a CMRR figure for input common mode voltage range of (V-) < VCM < (V+) - 1.3V however the VCM range is (V-) -0.1 to (V+) +0.1. I'm was wondering what the CMRR is for VCM > (V+) -1.3V and whether any problems would be seen in the circuit operation when operating above this upper VCM level.