Hi team,
According to the datasheet, it seems that the output impedance just increases to about 160kOhm while the device is disabled.
But are there any changes else while the device is disabled?
Regards,
Noriyuki Takahashi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
According to the datasheet, it seems that the output impedance just increases to about 160kOhm while the device is disabled.
But are there any changes else while the device is disabled?
Regards,
Noriyuki Takahashi
Hi team,
One more question.
Could you also tell what the output voltage can be while the device is disabled in case of adder circuit or Non-inverting amplifier circuit?
Regards,
Noriyuki Takahashi
Noriyuki,
When the amplifier is disabled the output stage is turned off. The output will float to a small voltage. If the output is connected to a load it will be pulled to the load voltage. The non-inverting input will remain as it was before disabling the output. I tested the functionality with the EVM using a adder circuit. Let me know if you have some specific additional questions. The EVM is useful for this kind of test. You may consider getting a copy. See attached PDF: opa462evm suming circuit.pdf
Best regards,
Art
Art,
Do you mean that the ouput voltage can be below in both non-inverting and a adder circuit?
1. When the amplifier is disabled, the output will float to a small voltage.
2. If the output is connected to a load it will be pulled to the load voltage.
If the output is connected to a load it will be pulled to the load voltage.
What do you mean the load voltage?
Do they need to take care of the loop stability in case of disabled, too to prevent the oscillation?
Regards,
Noriyuki Takahashi
Noriyuki,
I hope the additional detail below helps.
4300.opa462evm suming circuit2.pdf
Best regards,
Art