Hi team,
My customer is evaluating TLV9062IDR in their product and met below issue now, could you please give some comments and suggestions?
The capacitive load drive capability shown on the datasheet of the TLV9062IDR is 100pF, but when the actual output capacitance is 100pF, the output voltage is incorrect.
Normal theoretical calculation output voltage should be, from 1.07V to 1.27V, frequency 140KHZ, duty cycle approx. 0.8, increase slope 3.5*10^4 V/s.
Actual trapezoidal current: From 11.4A to 13.1A, frequency 140KHZ, duty cycle approx. 0.8, ramp up 0.296A/us.
Sample resistance value is 5mΩ, operational gain is 22, C482 capacitance is 220PF, C478 capacitance is 220PF.
The voltage of the sample resistance (i.e. the discharge input voltage) is increased from 57mV to 65.5mV at a frequency of 140KHZ, duty cycle approx. 0.8, ramp up 1487V/s, The actual output voltage is low.
The TLV9062 schematic is as follows: Gain: 22, C482 capacitance: 220PF, C478 capacitance: 220PF
After removing capacitance C482 in parallel with the negative feedback resistor, or reducing the capacitance to 20pF, the output voltage of TLV9062 is normal.
Thank you.
Regards,
Ivy