This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMV393: OVP/ UVP detect function

Part Number: LMV393


Hi Sir,

can customize the judgment potential solution conditions of OVP and UVP as follows:

1. When IN_A (OCP_H) voltage≧H_S, OUT_A is H, when IN_A voltage<H_S, OUT_A is L

2.When IN_B(OCP_L) voltage≦L_S, OUT_B is H, when IN_B voltage>L_S, OUT_B is L

3. Points 2 and 3 ic can be discrete or combo.

4. The currently evaluated ICs include Reset IC, analog switch IC, and comparator. Please kindly help evaluate the differences in this application.

maybe LMV393 can do it, right?