Part Number: OPA3S2859-EP
Other Parts Discussed in Thread: OPA3S2859
Hello TI experts,
I'm interested in using in the OPA3S2859 but need a few clarifications based on the datasheet specs:
Question 1. The datasheet is referring to three internal switched feedback paths, each switch is optimized for feedback resistor values ranging <1k to >100k. (page 1, 3, 4, etc).
Is it mandatory for the low gain feedback resistor to be < 1k? what is the minimum accepted resistor value?
Is it mandatory for the medium gain feedback resistor to be ~10k and for the high gain resistor to be > 100k?
Or can I use resistor values for LO/MED/HI of my choosing, for example, I'm looking to use this devices in a transimpedance (TIA) configuration for a photo diode where current varies from 0mA to 5.1mA with a target BW of 35MHz. I'm using the COMx input and I'm not connecting the IN- input.
I would like to be able to use resistors ranging from 300 ohm up to 1k so I would be far off from the 10k for medium and 100k for hi gain.
Is this possible? What concerns me is the RON_COMx spec on page 8 which appears to mention 375 ohm for RON_COM2, 125 ohm for RON_COM1 and 80 ohm for RON_COM0, considering the typical range of 300-600 ohm that I would like to use for our application.
Question 2. This device can be powered with supply range from 3.3V to 5.25V (page 1 of the datasheet) or -2.5V / +2.5V. The maximum output voltage of this device (Voh) is limited by the upper supply rail and is defined as 3.95V (min) for a 5V supply and 2.3V (min) for a 3.3V supply. I'm planning on using this device with bipolar supply but not with the above mentioned -2.5V / +2.5V but rather -1.5V / +3.5V in order to maximize the Voh and still be able to reach 0V output.
Is it possible to chose the +/- supply this way or can I only use the mentioned voltages from the datasheet: 3.3V to 5.25V or -2.5V/+2.5V? The datasheet briefly mentions that unbalanced bipolar supply operation is supported but does not provide further details (page 22, chapter 10).
Question 3. The datasheet specifies a maximum Iin (continuous input current) of +/-4mA. In our application we have a DC component in the current of 2.5mA and an AC component of 2.5mA (non-continuous). So total max can be 5.1mA based on a signal that varies up to 35MHz. Is this sort of input allowable or would this violate the "+/-4mA continuous spec"?
Thanks for the support!
Best,
Peter