This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS6424EQ1EVM: Power Dissipation vs Output Power - Environment Setup

Part Number: TAS6424EQ1EVM


Hi,

I'm reviewing the specifications for a TI Amplifier (TAS6424EQ1EVM) and have some questions I'd like to clarify. Could you please provide more information on the following?

1. Regarding the temperature conditions Ta=25°C and Tc=75°C specified in the datasheet, are these temperatures constantly maintained during the testing process for accurate measurements?

2. Is it correct to say that all power dissipation ultimately gets converted into heat?

Thank you for your assistance.

Best regards,
Jeffery.