Other Parts Discussed in Thread: AMC3330
Hello Sir:
I'm not sure how to understand the CLR and CPG parameters.
Because I check the package footprint, the pin clearance is around 7.6mm.
And AMC3330Q1 spec shows CLR and CPG ≥8mm, and which can works on 1700VDC.
According to IEC 60664-1, material group II which minimum creepage distance should be around 11mm on 1600V application.
Would you please explanation this gap between TI datasheet and IEC 60664-1 rule?
And how to understand these two parameters?
Looking forward your feedback.
Thanks a lot.