The datasheet of INA818 discribes two equations, G=1 + 50k/Rg and Vo=G*(Vin- - Vin+).
When I select Rg=239, G=1 + 50k/239 = about 26 and Vo=26*(Vin- - Vin+).
Then, when I measured Vo in Vin-=-0.3 and Vin+=4.7 (Vdiff=-5.0 V), this actual value is almost same as the expected value (-14.85 V caluclated by Analog Engineer's Caluclator).
It seems that INA818 works correctly in this condition (very high Vdiff), but some amplifier has a range of defferential input voltage.
Does INA818 have absolute maximum ratings of defferential input voltage?