Part Number: OPA4991-Q1
Other Parts Discussed in Thread: OPA4991
Hello,
I am designing OP AMP circuit that circuit uses OPA4991-Q1.
I will use OPA4991-Q1 for voltage follower circuit under below conditions.
IN+ pin : Connect 4/5 voltage divider resistors (100kohm and 25kohm)
* Input signal for voltage divider circuit : 20Vp-p 1kHz sine wave signal (Offset voltage: 0V)
IN- pin : Connect OUT pin through 20kohm feed back resistor.
* To cancel out effect of input offset current effect : value of 100kohm // 25kohm = 20kohm
I would like to confirm maximum limit of feedback resistor value for voltage follower circuit using OPA4991-Q1.
I am concerned that too large feedback resistor value will affect the operation of the OP AMP circuit.
Regards,
MESH