This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV2186: input bias to +45°C

Genius 17355 points

Part Number: TLV2186

Hi all

My customer is evaluating the TLV2186 in an application where the operating temperature of the device will go to max +45°C and they have this question:

Can you provide more detailed data on the input bias current up to +45°C ? 

From figure 9 in the datasheet one cannot judge the range of the input bias at lower temperatures.

Best regards

Ueli