This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV9302: Increament of Slew Rate in Op-Amp.

Part Number: TLV9302
Other Parts Discussed in Thread: TLV9362, TLV9352, OPA2992

Hi there,

I'm using TLV9302 (Rail to Rail) opamp.+12V & -12V given as supply voltage. PWM pulse of 1KHZ given as input at 16ns time period. At Op-Amp's output we get 5us. 3V/us is OP-Amps output side rise timementioned in datasheet.Can we increase slew rate, so that the rise time would reduse. under 2us is desired outcome.