Part Number: TL081H
I have a scenario where the TL081H will be supplied with a 18 VDC single voltage supply (Vss to GND). The output of this device goes to an external connector that is required to meet voltage transient specifications. From an LTSpice simulation it would appear as if the voltage transient on the output of the device can go as high as 24VDC for a duration of roughly 250us
Will the device be able to withstand such a transient? The datasheet specifies input port common mode voltage maximums of Vcc+0.5V, which if it was the same for the output port, would certainly lead to damage. Does the output operate under the same limits as the input and is there a transient duration that will allow for the maximum to be uprated to a high value such as this case where is transient duration is < 250us

Regards,
Jason