This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA810: Please recommend a amplifier

Part Number: OPA810


I am targeting use below adc circuit to measure external transient by resistor devider.

So I need to use OP for the front for OP follower circuit.

The target application is for 1MHz signal.

The front end resistor divider is 950K + 50K ohm

Could you recommend a suitable amplifer?