Other Parts Discussed in Thread: TINA-TI, PSPICE-FOR-TI
Hello,
I'm trying to simulate the OPA3S328 using the provided spice model in LT Spice XVII.
I wired the circuit exactly like the figure 1-1 in the sboa521 application note. When I run a simple .op simulation for DC operating point I get the following error in the SPICE log:
WARNING: Less than two connections to node U1:_OPA3S328_SWITCH:_U24:_U1:NVCC. This node is used by E:U1:_OPA3S328_SWITCH:_U24:_U1:V.
WARNING: Less than two connections to node U1:_OPA3S328_SWITCH:_U22:_U1:NVCC. This node is used by E:U1:_OPA3S328_SWITCH:_U22:_U1:V.
WARNING: Less than two connections to node U1:_OPA3S328_SWITCH:_U25:_U1:NVCC. This node is used by E:U1:_OPA3S328_SWITCH:_U25:_U1:V.
WARNING: Less than two connections to node U1:_OPA3S328_SWITCH:_U23:_U1:NVCC. This node is used by E:U1:_OPA3S328_SWITCH:_U23:_U1:V.
WARNING: Less than two connections to node U1:_OPA3S328_SWITCH:_U26:_U1:NVCC. This node is used by E:U1:_OPA3S328_SWITCH:_U26:_U1:V.
WARNING: Less than two connections to node U1:_OPA3S328_SWITCH:_U27:_U1:NVCC. This node is used by E:U1:_OPA3S328_SWITCH:_U27:_U1:V.
This seems to be internal to the model and the problem seems to happen only when the included analog switch are part of the feed back loop. If I don't include the switch in the amplifier feedback loop everything works even the switch themselves.
Can anyone validate if the model is correct?
Thanks