Hi,
We use the attached circuit in one of our products. In some cases the wiper of a potentiometer connected between +5V and ground is connected to IN1, but in most cases no potentiometer is connected. I have found that when no pot. is connected input IN1 tends to drift below +5V on some devices, evidenced by OUT1 voltage dropping, so I believe the original designer did not bias U1A properly.
My understanding is that the common mode input range for the LMV932MAX/NOPB includes VCC (+5V). A short term fix is to connect IN1 to +5V, which seems to work, but I would like to know if there are any long-term negative effects in doing this.
Ideally I think it would be best to bias IN1 at about +4V using a resistor divider, but I don't have pads on the board for another resistor. Can you tell me if using a lower value resistor for R1 would work, and how to calculate the best value?
Thanks in advance,
Bill