Can the TLV9054 create an active filter with the following parameters: 75kHz curry freq, 50kHz bandwidth. Gain 3dB. around -20dB at 160kHz?
From initial calculation, it appears we will need two stages for the above filter requirements and the second stage would need a higher bandwidth (~11.6Mhz). Can you please confirm and let me know if there are any other key specifications to consider?
Thanks,