This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM358: Output clamped at 9.63V with 3.5 noninverting gain.

Part Number: LM358

I have a LM358 in a non-inverting setup with a 12V supply. I have observed a gain of around 3.5 using a 200 ohm and 75-ohm resistor, however the output clamps around 9.63V even though the power supply is at 12V. Is there a max output specification I am unaware of? I appreciate the help. Thank you.