This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA188: looking for similar spec with INA188 but have higher slew rate

Part Number: INA188
Other Parts Discussed in Thread: INA821, INA828

Dear team,

Customer have design INA188 in their system but looking for similar spec and with higher slew rate solution.

Could you share your suggestion with us? Thanks.

If you have two more different slew rate level can offer to customer for option, that will be better.

 

Regards,

Ben

  • Hello Ben,

    The INA828 is a higher performing part that provides faster slew rate and higher bandwidth, for highest performance there is the INA821, with the widest bandwidth and fastest slew rate. 

    An parametric comparison is available here for all three devices

    Part INA188 INA828 INA821
    CH 1 1 1
    Vmin 4 4.5 4.5
    Vmax 36 36 36
    SR [G=min, typ] (V/µs) 0.9 1.2 2
    GBW [G=min, typ] (MHz) 0.6 2 4.7
    CMRR [G=max, min] 118 140 140
    Vos [25⁰C, max] (µV) 55 50 35
    Iq [typ] (mA) 1.4 0.6 0.6
    Vn [typ, 1KHz] (nv/√Hz) 12.5 7 7
    Vdrift [-40⁰C to 125⁰C, max] (µV/⁰C) 0.2 0.5 0.4
    Ib [25⁰C, Vcm = Vs/2, max] (nA) 2.5 0.6 0.5

    Regards,

    Cynthia