Part Number: LMV358A
Other Parts Discussed in Thread: TPS62A01
I have a few questions about overvoltage on the input of the LMV358A op-amp. I watched one of TI's videos on this subject, and here is a screenshot from the video:

In this diagram, are the TVS diodes included because the +/- 15V supply is a linear regulator, and linear regulators are unable to sink the current? If a buck regulator is used, would the current have a path to ground? I will be using the TPS62A01, which operates in forced PWM all of the time. The block diagram of the device shows high and low-side FETs, so it seems if the output voltage rises, the low-side FET would turn on more often which would pull current out of the inductor. But that process may be slow, so is that the reason for needing the TVS diodes?
I don't need high accuracy, so I am willing to use a very high-valued series resistor in the signal path, such as 1 MOhm. This would greatly reduce the current, even for voltages of several hundred volts. How low would the current need to be in order to allow the Absorption Device in the op-amp to absorb the extra current, making the TVS diodes unnecessary?
Since the LMV358A has some internal ESD protection, will a 1M series pulse-proof resistor on the input be sufficient to prevent ESD from being an issue? Or would I need to add a TVS diode on the input as well?
Thank you for the help.
Best regards,
Greg