Other Parts Discussed in Thread: OPA211,
Hi,
I'm using the HT part (will be at +125C operating temp.) in a fly-back power supply feedback loop, configured as a differential amplifer - the bandwidth is a maximum of 400 kHz.
The gain is set at -0.2 (-14dB) which is to ensure the input voltages never exceed their limits. While the circuit is stable and performs well, I'd welcome a full GBW plot as I'd like to ensure the device is (on paper at least) stable at such a low gain.
Thank you,
BR
Cole