Part Number: INA199
I have an INA199B3DCKR that is measuring the current through a 1 Ohm resistor, the current varies between 0 to 120mA.
I have confirmed that I'm getting the expected voltage drop across the 1 Ohm resistor but the output of the INA199 is always 0.03V.
The IN+ is ~24V and the IN- is ~23.88V. In+ and IN- will both occasionally drop to 0V. Is that my problem?
The reference pin is tied to 0V
The layout of the chip is shown below.