Hi
Only absolute max.voltage on input pins are listed in opa 4197。What is maximum voltage for Vout pins?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Only absolute max.voltage on input pins are listed in opa 4197。What is maximum voltage for Vout pins?
Hi Ken,
The output pins have ESD cells connected to the supply pins, just like the inputs.
In order to avoid any excessive conduction through the ESD cells, the voltage at the output must not exceed 0.5 V above the positive supply (Vdd + 0.5 V) or below the negative supply (Vss - 0.5 V).
Let me know if there's any further questions.
Regards,
Mike