Other Parts Discussed in Thread: TMUX6208, OPA140
Hi,
We have a circuit consisting of a OPAMP (OPA145) and AMUX (TMUX6208). The input of the OPAMP is connected to a mother-board test point. When there is no voltage from the mother board, we are getting some random voltage (from 1-3V) at the Input (pin 3) and Output (pin 1) of the OPAMP. Below is the circuit for your reference.
So, this random voltage might damage the mother board as this is connected to the test point of the motherboard. Also, as the same voltage is going to the AMUX, we are getting some voltages at the ADC even there is no voltage from the motherboard through the test point.
Could you please suggest some solution so that we can avoid this issue.
Thanks.