Other Parts Discussed in Thread: INA302, INA303, INA234, INA181
Hello,
I have a question about the hysteresis of the INA301. Do to design specifications, I would like to use the A3 reference with a Vlimit of 50mV. Nevertheless, the datasheet says that it's hysteresis is 100mV, does it mean that once activated, the ALARM signal will not be deactivated again?
If so, could it be a way to deactivate the hysteresis?
Maybe, under a minimum difference the hysteresis is not workin?
I have not see a minimum for Vlimit, but if there is no posibility for deactivate the output if the Vlimit<100mV, I consider that it should be mentioned somwhere.
Thank you in advance and best regards.
Egoitz.