Other Parts Discussed in Thread: VCA824, THS3091, THS6204, PGA870, TLC7524, TL074, TINA-TI, LMH6554, LMH6523
Hello,
I need to implement a variable voltage output amplifier....digitally controlled output voltage is ideal
the output needs to be a square wave of 3.3V to 20v - the input is a 3.3v square wave
the max frequency output ~1Mhz
the rise and fall time needs to be ~10ns (monotonic) with an output set at 5V
the power supply is 24V
any suggestions you can provide? any app notes available?
SR