The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2310: Absolute Maximum Supply Voltage Discrepancy

Part Number: OPA2310

For the OPA2310, in datasheet section 7.1 the absolute maximum supply voltage [ Vs = (V+) - (V-) ] is listed as 7V. However, later in datasheet section 9.3 a caution box suggests that supply voltages larger than 6V can permanently damage the device.

Now, I have seen this same caution box in similar TI chip datasheets, so maybe it is a copy paste error. Or could the 7V absolute maximum be an error? I am hoping a TI expert could help sort this out.

For more context, we are hoping to use the OPA2310 running with a 6V supply voltage (+3V and -3V). Yes the recommended limit is 5.5V, but we have struggled to find a component that meets a demanding list of constraints. If the OPA2310 can safely run at 6V, below an absolute limit of 7V, then we are in the clear. (Our signal pin voltages are much lower; no other absolute maximum rating is a problem)

Thanks for your time.