Other Parts Discussed in Thread: XTR111,
I am designing an iepe signal conditioner and as seen in the introduction I have a 2nd order butterworth high pass filter..
When the sensor (load) is not connected, the current source with 24 V supply with 4mA constant current will completely turn on the MOSFET and the output will be 24 volts (xtr111 output will not give exactly 24 volts, it will give a value of approximately 21.6V), but let's assume that there is a 24V input.
-----------------------------------------------------------------------------------------------------------------------------
If we look at the OPA192 datasheet, the entry values in the Absolute Maximum Ratings section are limited as follows. Since we are supplying (V–) – 0.5 and (V+) + 0.5 :(+15V )(-15V ), -15.5 and 15.5 are the maximum limits we can apply to the inputs
.
-----------------------------------------------------------------------------------------------------------------------------
If we focus on transient analysis, when the 24V input signal comes, the current will pass through the clamp diode (BAT64) through the 2k limiting resistor and go to the +15 line. The simulation is here.
Accordingly, the 15V power supply will need to sink a value such as 3.315mA. I use a UWE1215S-3WR3 supply that can output +-15 V to feed the opamp. However, I am not sure how much source sinking it can do, maybe it does not do it at all.
graph of the +15 volt source
u can see the +15v source is sinking You can see that it is sinking for up to 10ms.
Briefly, how can I protect the inputs of the opamp when we apply 24v? Do I need to add a 15V zener diode reverse connected to the power rails for sinking?
I don't want the opamp to burn out when there is no load.
If you notice any other errors in the circuit, please let me know.