Part Number: TL084
Dear Specialists,
I'm considering the application note (SPRABY3) for calculating kai square (confidence level(%), degree of freedom)
To begin with,
As stated in equation (2), even if the confidence level of 60% and degree of freedom (2*1+2) are set, Kai Square (60%, 2x1+1) does not become 0.917.
When 0.917 was used in the calculation example, the FIT values were almost the same value(50.5).
Assuming 0 failures from 231 samples for 1000 hours HTOL @ 125°C, the FIT would calculate to be 50.9 FIT with 60% CL at 55°C.
Could you please let me know where I am wrong.
What we actually want is the value of Kai Square at the confidence level of 70%.
I appreciate your great help in advance.
Best regards,
Shinichi