Hi,
We are using INA310A3-Q1 for one of our application. I would like to know whether the trip voltage (close to 0.6V) can be set only with Vsense & gain without the use of divider resistors. In datasheet, I couldn't see the option to set trip limit without the divider resistors.
Eg: If my normal Vsense is 2.5mV, with a gain of 50, gives 0.125V & for sense voltage of 12.5mV (trip), with a gain of 50, gives 0.625V (crosses comparator reference of 0.6V). By this way can I implement the over current trip without using the divider resistors ??
Kindly clarify.
Thanks in advance.
Prahaladh S