Part Number: XTR110
Hi all. I am planning on using the XTR110 as a simple 0-10V to 4-20mA converter, and would like to use a surface-mount external transistor. The recommended transistors in the datasheet are all through-hole, and most of them seem to be obsolete.
Apart from ensuring Vds is greater than my supply voltage, and Pd is high enough, are there any other specs that I should be looking at for the PMOS? Rds On? Vgs th?
The supply voltage will be 28VDC.
Would both the of the following be acceptable?
- Diodes Incorporated DMP10H400SK3
- Vishay Siliconix SUD09P10-195
Thanks!