This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XTR110: Recommendation for SMD external transistor

Part Number: XTR110

Hi all. I am planning on using the XTR110 as a simple 0-10V to 4-20mA converter, and would like to use a surface-mount external transistor. The recommended transistors in the datasheet are all through-hole, and most of them seem to be obsolete.

Apart from ensuring Vds is greater than my supply voltage, and Pd is high enough, are there any other specs that I should be looking at for the PMOS? Rds On? Vgs th?

The supply voltage will be 28VDC.

Would both the of the following be acceptable?

  • Diodes Incorporated DMP10H400SK3
  • Vishay Siliconix SUD09P10-195

Thanks!