Other Parts Discussed in Thread: LM6132, OPA928
Hi,
we are designing a new analog frontend and plan to use the OPA392 because of its very low input bias.
Unfortunately, the absolute max supply voltage for the OPA392 is +/-3V. In rare cases, our input signals can reach up to +/-7V.
Now we are curious if it's possible to limit the current to below 10mA using a series resistor and the OPA392 will still be fine?

Other devices like the LM6132 have similar characteristics regarding their Inputs pins, but the datasheet clearly states, that it's possible:
"The LM6132/34 can be driven by voltages that exceed both power supply rails, thus eliminating concerns over exceeding the common-mode voltage range"

We assume that the OPA392 is equipped with internal clamping diodes, so if the input voltage exceeds the supply voltage but limited to 10mA using a series resistor, there should be no damage?
Thanks,
Heiko