This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6629: Ultra small photodiode AC current amplification (2 MHz) using TIA

Part Number: LMH6629
Other Parts Discussed in Thread: OPA855, OPA858

Dear Specialists and TI users, 

In past when implementing Photodiode amplification stage for VLC I usually used a transimpedance amplifier such LMH6629 and then use a high speed comparator set at Vref. 

However here I need to amplify very small current at the order of nA or tens of nA from S1223 Photodiode (Cp = 10pF) and remove DC bias. For such small current the voltage variation at the output of the TIA is too small in order to connect directly the comparator. 

I tought to use Voltage amplifier in cascade but I am afraid of the noise figure and also would tought how removing DC bias regarding ultra small AC variation (f=2MHz). 

If possible for you of course, I would really appreciate to have your advice on these question. 

I wish you a nice day, 

Yours, 

Simon