This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV9054: Input voltage above abs max

Part Number: TLV9054


Hello team,

Can I input higher voltage than abs max for the input pin (+IN)?
When I power down the device, the input voltage stays high, and exceed the abs max by 0.1V for short amount of time.

There is ESD diode from +IN to V+, so as long as I limit the input current under 10mA, is it okay to exceed abs max voltage for +IN?

Best Regards,
Kei Kuwahara