Other Parts Discussed in Thread: PGA281, MUX36D08
Hello TI,
We're using the current sources on the PGA280 with great success to measure an estimate of loop resistance. It's working very well for loops of less than ~20K Ohm.
As we're approaching higher resistance loops, however, we're finding that the current sources seem to have trouble once their voltage is more than about +/-1.25V or 2.5V total.
Being that they're connected to VSP and VSN (which, in our circuit are +/-18V), I would have expected them to easily drive, say +/-15V for a 30V potential.
Does this seem correct? I can find nothing in the datasheet that would lead me to believe this should be the case.
To summarize, no matter how much resistance we connect across INP1 and INP2, when F1 and F2 are turned on, the maximum voltage output by the current sources seems to be around 2.5V.
We have also tried F1/G2 and F2/G1, and the result is roughly the same - ~2.5V at the PGA output in GAIN=1
Appreciate any insight.
Ben