This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV7022: Negative voltage transient

Part Number: TLV7022

Hi team,

Could you please check if the ~-1V ~100ns negative voltage transient at input pin should be okay for TLV7022?

VEE=0V.

Will it parmanently damage the device?

My customer is seeing such a negative transient on the test.

If it is problem, I will ask the customer to limit the current <10mA following the datasheet.

Best regards,

Kazuki Itoh