Is it necessary to add a voltage buffer to the output to input into an ADC? The output amplifier has an output of almost 10mA (Figure 7). It appears that a buffer is not needed. Is that correct? Is there a reason to add a voltage follower buffer between the output of the INA901-SP and an ADC?